Instrument Control (INSTR) Resource Events
                                                         
                                                     | 
                                                    
                                                         This version of the IO Libraries Suite supports Windows and Linux. Available utilities, APIs, help files and features vary by operating system. Variations are flagged in help with these icons:   | 
                                                
In the following tables, AP = Access Privilege, RO - Read Only, and RW = Read/Write.
VI_EVENT_SERVICE_REQUEST
Notification that a service request was received from the device.
Supported: 

| 
                                                         Event Attribute  | 
                                                    
                                                         Attribute Value  | 
                                                    
                                                         Description  | 
                                                    
                                                         AP  | 
                                                    
                                                         Data Type  | 
                                                    
                                                         Range  | 
                                                
|---|---|---|---|---|---|
| 
                                                         VI_ATTR_EVENT_TYPE  | 
                                                    0x3FFF4010UL | 
                                                         Unique logical identifier of the event.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViEventType  | 
                                                    
                                                         VI_EVENT_SERVICE_REQ  | 
                                                
VI_EVENT_VXI_SIGP
Notification that a VXIbus signal or VXIbus interrupt was received from the device.
Supported: 
 (Windows only)
| 
                                                         Event Attribute  | 
                                                    
                                                         Attribute Value  | 
                                                    
                                                         Description  | 
                                                    
                                                         AP  | 
                                                    
                                                         Data Type  | 
                                                    
                                                         Range  | 
                                                
|---|---|---|---|---|---|
| 
                                                         VI_ATTR_EVENT_TYPE  | 
                                                    0x3FFF4010UL | 
                                                         Unique logical identifier of the event.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViEventType  | 
                                                    
                                                         VI_EVENT_VXI_SIGP  | 
                                                
| 
                                                         VI_ATTR_SIGP_STATUS_ID  | 
                                                    0x3FFF4011UL | 
                                                         The 16-bit Status/ID value retrieved during the IACK cycle or from the Signal register.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViUInt16  | 
                                                    
                                                         0 to FFFFh 
  | 
                                                
VI_EVENT_TRIG
Notification that a trigger interrupt was received from the device. For VISA, the only triggers that can be sensed are VXI hardware triggers on the assertion edge (SYNC and ON trigger protocols only).
Supported: 

| 
                                                         Event Attribute  | 
                                                    
                                                         Attribute Value  | 
                                                    
                                                         Description  | 
                                                    
                                                         AP  | 
                                                    
                                                         Data Type  | 
                                                    
                                                         Range  | 
                                                
|---|---|---|---|---|---|
| 
                                                         VI_ATTR_EVENT_TYPE  | 
                                                    0x3FFF4010UL | 
                                                         Unique logical identifier of the event.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViEventType  | 
                                                    
                                                         VI_EVENT_TRIG  | 
                                                
| 
                                                         VI_ATTR_RECV_TRIG_ID  | 
                                                    0x3FFF4012UL | 
                                                         The identifier of the triggering mechanism on which the specified trigger event was received.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViInt16  | 
                                                    
                                                         VI_TRIG_TTL0 to VI_TRIG_TTL11;   | 
                                                
* Keysight VISA can also return VI_TRIG_PANEL_IN (exception to the VISA Specification).
VI_EVENT_IO_COMPLETION
Notification that an asynchronous operation has completed.
Supported: 

| 
                                                         Event Attribute  | 
                                                    
                                                         Attribute Value  | 
                                                    
                                                         Description  | 
                                                    
                                                         AP  | 
                                                    
                                                         Data Type  | 
                                                    
                                                         Range  | 
                                                
|---|---|---|---|---|---|
| 
                                                         VI_ATTR_EVENT_TYPE  | 
                                                    0x3FFF4010UL | 
                                                         Unique logical identifier of the event.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViEventType  | 
                                                    
                                                         VI_EVENT_IO_COMPLETION  | 
                                                
| 
                                                         VI_ATTR_STATUS  | 
                                                    0x3FFF4025UL | 
                                                         Return code of the asynchronous I/O operation that has completed.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViStatus  | 
                                                    
                                                         N/A  | 
                                                
| 
                                                         VI_ATTR_JOB_ID  | 
                                                    0x3FFF4006UL | 
                                                         Job ID of the asynchronous operation that has completed.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViJobId  | 
                                                    
                                                         N/A  | 
                                                
| 
                                                         VI_ATTR_BUFFER  | 
                                                    0x3FFF4027UL | 
                                                         Address of a buffer that was used in an asynchronous operation.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViBuf  | 
                                                    
                                                         N/A  | 
                                                
| 
                                                         VI_ATTR_RET_COUNT  | 
                                                    
                                                         32-bit: 0x3FFF4026UL 64-bit: 0x3FFF4028UL  | 
                                                    
                                                         Actual number of elements that were asynchronously transferred.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViUInt32  | 
                                                    
                                                         0 to FFFFFFFFh  | 
                                                
| 
                                                         VI_ATTR_OPER_NAME  | 
                                                    0xBFFF4042UL | 
                                                         Name of the operation generating the event.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViString  | 
                                                    
                                                         N/A  | 
                                                
| 
                                                         VI_ATTR_RET_COUNT_32  | 
                                                    0x3FFF4026UL | 
                                                         Actual number of elements that were asynchronously transferred.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViUInt32  | 
                                                    
                                                         0 to FFFFFFFFh  | 
                                                
| 
                                                         VI_ATTR_RET_COUNT_64*  | 
                                                    0x3FFF4028UL | 
                                                         Actual number of elements that were asynchronously transferred.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViUInt64  | 
                                                    
                                                         0 to FFFFFFFFFFFFFFFFh  | 
                                                
*Defined only for frameworks that are 64-bit native.
VI_EVENT_USB_INTR
Notification that a vendor-specific USB interrupt was received from the device.
Supported: 

| 
                                                         Event Attribute  | 
                                                    
                                                         Attribute Value  | 
                                                    
                                                         Description  | 
                                                    
                                                         AP  | 
                                                    
                                                         Data Type  | 
                                                    
                                                         Range  | 
                                                
|---|---|---|---|---|---|
| 
                                                         VI_ATTR_EVENT_TYPE  | 
                                                    0x3FFF4010UL | 
                                                         Unique logical identifier of the event.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViEventType 
  | 
                                                    
                                                         VI_EVENT_USB_INTR  | 
                                                
| 
                                                         VI_ATTR_USB_RECV_INTR_SIZE 
  | 
                                                    0x3FFF41B0UL | 
                                                         Specifies the size of the data that was received from the USB interrupt-IN pipe. This value will never be larger than the sessions value of VI_ATTR_  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViUInt16  | 
                                                    
                                                         0 to FFFFh  | 
                                                
| 
                                                         VI_ATTR_USB_RECV_INTR_DATA  | 
                                                    0xBFFF41B1UL | 
                                                         Specifies the actual data that was received from the USB interrupt-IN pipe. Querying this attribute copies the contents of the data to the users buffer. The users buffer must be sufficiently large enough to hold all of the data.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViBuf  | 
                                                    
                                                         N/A  | 
                                                
| 
                                                         VI_ATTR_STATUS  | 
                                                    0x3FFF4025UL | 
                                                         Specifies the status of the read operation from the USB interrupt-IN pipe. If the device sent more data than the user specified in VI_ATTR_USB_MAX_INTR_SIZE, then this attribute value will contain an error code.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViStatus  | 
                                                    
                                                         N/A  | 
                                                
VI_EVENT_PXI_INTR
Notification that a PCI Interrupt was received from the device.
Supported: 
 (Windows only)
| 
                                                         Event Attribute  | 
                                                    
                                                         Attribute Value  | 
                                                    
                                                         Description  | 
                                                    
                                                         AP  | 
                                                    
                                                         Data Type  | 
                                                    
                                                         Range  | 
                                                
|---|---|---|---|---|---|
| 
                                                         VI_ATTR_EVENT_TYPE  | 
                                                    0x3FFF4010UL | 
                                                         PCI Interrupt was received from the device.  | 
                                                    
                                                         RO  | 
                                                    
                                                         ViEventType  | 
                                                    
                                                         VI_EVENT_PXI_INTR  | 
                                                
VI_EVENT_VXI_VME_INTR (NOT IMPLEMENTED)
- Notification that a VXIbus interrupt was received from the device.
NOT IMPLEMENTED IN KEYSIGHT VISA.
| 
                                                     Event Attribute  | 
                                                
                                                     Attribute Value  | 
                                                
                                                     Description  | 
                                                
                                                     AP  | 
                                                
                                                     Data Type  | 
                                                
                                                     Range  | 
                                            
|---|---|---|---|---|---|
| 
                                                     VI_ATTR_EVENT_TYPE  | 
                                                0x3FFF4010UL | 
                                                     Unique logical identifier of the event.  | 
                                                
                                                     RO  | 
                                                
                                                     ViEventType  | 
                                                
                                                     VI_EVENT_VXI_VME_INTR  | 
                                            
| 
                                                    
                                                     
  | 
                                                0x3FFF4041UL | 
                                                     VXI interrupt level on which the interrupt was received.  | 
                                                
                                                     RO  | 
                                                
                                                     VIInt16  | 
                                                
                                                     1 to 7, VI_UNKNOWN_LEVEL  | 
                                            
| 0x3FFF4023UL | 
                                                     32-bit status/ID retrieved during the IACK cycle.  | 
                                                
                                                     RO  | 
                                                
                                                     ViUInt32  | 
                                                
                                                     0 to FFFFFFFFh  | 
                                            
See also: Instrument Control (INSTR) Resource.